Guide to electrical tape colours
Electrical tape, also known as electrical insulation tape – or just insulation tape – it’s typically made of flexible materials such as vinyl or PVC. One side of the tape is coated with a pressure-sensitive adhesive. This allows the tape to adhere firmly when applied to surfaces. This guide is designed to help you understand what colour electrical tape to use and the tape colour meaning. We’ll cover:
What is electrical tape for?
The Basics of Electrical Tape Colours: What They Mean
Common Electrical Tape Colours and Their Significance
Safety Precautions When Working with Electrical Tape of Different Colours
What is electrical tape for?
The purpose of electrical tape is to insulate and protect electrical connections, wires, and cables. Another function of electrical tape is to prevent electrical shocks or short circuits. By wrapping the tape around exposed conductors or connections, it creates a barrier that shields them from moisture, dust, and other contaminants. This not only ensures safety but also helps maintain the integrity of the electrical system.
The Basics of Electrical Tape Colours: What They Mean
Electrical tape uses also include colour coding and marking. More accurately, this is called phasing tape, or sometimes phase tape.
What is phase tape? Electrical tape is technically a general-purpose tape. Phase taping is a type of electrical tape used to identify and mark different phases or conductors in electrical systems. So is red tape electrical tape? Technically, it’s a phase tape. Phase tape is specifically used in situations where multiple voltage-carrying conductors or phases need to be distinguished from one another.
The primary purpose of phasing tape is to provide a visual indication and aid in the identification of specific phases, ensuring proper installation, maintenance, and troubleshooting of electrical circuits. By applying phasing tape to individual conductors, electricians and technicians can easily differentiate between the different phases, reducing the risk of errors or confusion.
Phasing tape is typically colour-coded, with each colour representing a specific phase. In the UK, there are typically 3 phase colours used for electrical installations. As it’s better known as electrical tape, that’s the name we’ll use here. The tapes common in the UK are:
● Red electrical tape
● Yellow electrical tape
● Blue electrical tape
These colours are used to identify different phases of electrical power, allowing for proper identification and organisation of wiring systems. The U.S. uses additional insulation tape colours, which are sometimes used in the UK – green electrical tape is an example. Grey electrical tape is rare in the UK. So is orange electrical tape. Brown electrical tape and purple electrical tape – also known as violet electrical tape – are used in the U.S., but not in the UK. And of course, the meaning of these tapes vary by region. A good example is white phase tape.
Common Electrical Tape Colours and Their Significance
Each colour has a purpose. First, black electrical tape is generally used to insulate electrical wires. But what is blue electrical tape used for? What is yellow electrical tape used for? And what is red electrical tape used for? These and other colours – the phasing tapes – indicate the voltage level and phase of the wire. Phasing tapes are used on wires that only come with black insulation. If those wires need to be phased, a ring of tape is placed on each end near the termination to make the purpose of the wire known. See below for electrical tape colours’ uses and meanings.
Electrical tape colour code chart
|
Colour |
Usage (UK) |
Usage (U.S.) |
Usage (International, new) |
|
Black tape |
Insulation /low voltage, neutral |
Insulation / low voltage, phase A |
Low voltage, phase B |
|
Red |
Low voltage, phase A |
Low voltage, phase B |
Sheath, 415 V 3 phase |
|
Blue |
Low voltage, phase C |
Low voltage, phase C |
Low voltage, neutral Sheath, 230 V |
|
Brown |
|
High voltage, phase A |
Low voltage, phase A |
|
Orange |
|
High voltage, phase B |
Colour of wiring sheath |
|
Yellow |
Low voltage, phase B |
High voltage, phase C |
Sheath, 110 V Site wiring |
|
Green |
Earth |
Earth ground |
|
|
Green with yellow stripe |
Earth |
Isolated ground |
Earth |
|
White |
Same purpose as black tape, but used to improve appearance for domestic appliances with white cords. |
Low voltage, neutral |
|
|
Grey |
Low voltage, phase C (Rarely used) |
Low voltage, phase C |
High voltage, neutral |
|
Purple |
|
High voltage, phase B |
|
Safety Precautions When Working with Electrical Tape of Different Colours
Safety precautions should be followed when working with electrical tapes. Here are important guidelines to consider:
1. Proper colour selection: Choose the appropriate colour of electrical tape based on its intended use, ensuring compliance with industry standards. For example, yellow insulation tape has a specific purpose.
2. Before use of electrical tape: Carefully examine it for any signs of damage such as cuts, tears, or issues with the adhesive. Do not use tape that is compromised or defective, as it may not provide sufficient insulation.
3. Adequate surface preparation: Prepare the surface where the tape will be applied by ensuring it is clean, dry, and free from any contaminants. This helps ensure a secure and effective bond between the tape and the surface.
4. Proper usage: Use tape for electrical wires only for its intended applications, such as insulating wires, bundling cables, or marking.
5. Correct application technique: When applying coloured insulation tape, wrap it tightly around wires or cables with appropriate tension. This ensures a secure and uniform insulation layer.
6. Layer overlapping: If applying multiple layers of yellow and green electrical tape – or any colour –, make sure each layer overlaps the previous one by at least half its width. This creates a reliable insulation barrier.
7. Avoid overstretching: While tension is important, avoid stretching the tape excessively, as it may lead to thinning and compromised insulation properties.
8. Verification of insulation integrity: After applying the tape, carefully inspect for any gaps or exposed wires. Ensure that all connections and exposed conductors are properly insulated.
Remember, coloured electrical tape is just one element of electrical safety. Always follow proper electrical practices and take necessary precautions to ensure a safe working environment.
Download free CADs and try before you buy
Free CADs are available for most solutions, which you can download. You can also request free samples to make sure you’ve chosen exactly what you need. If you’re not quite sure which solution will work best for your application, our experts are always happy to advise you.
Whatever your requirements, you can depend on fast despatch. Request your free samples or download free CADs now.
Questions?
Email us at sales@essentracomponents.co.uk or speak to one of our experts for further information on the ideal solution for your application 0345 528 0474.